PC-based control for intelligent control of heating, ventilation and air conditioning systems

The control of heating, ventilation and air conditioning systems is very important in building automation, both concerning the well-being of the user and the reduction of energy consumption as well as in protecting the building itself. Alongside the standard hardware portfolio for integration of all data points, Beckhoff provides the software tool TF8040 TwinCAT 3 Building Automation that covers the entire scope of functions of an intelligent HVAC control system.

The TwinCAT 3 Building Automation software library offers programmers and users the following benefits: efficient parameterization and commissioning, a consistently high level of system functionality, good readability and expandability of programs, ease of maintenance over many years, flexible expandability of systems, improved reusability of templates for plants or plant aggregates modules, easy training of service personnel, definition of a clear, object-oriented program structure, and good documentability of programs.

The modular range of automation components from Beckhoff offers scalable control components in all performance classes and designs, which can be used to configure needs-based control platforms for HVAC systems.
The modular range of automation components from Beckhoff offers scalable control components in all performance classes and designs, which can be used to configure needs-based control platforms for HVAC systems.

Further information about our technologies and products for controlling heating, ventilation and air conditioning can be found here:

Application reports and brochures

  • Create ultimate guest experiences! PC-based control for the entertainment industry
    01.08.2025 | Brochure

    Create ultimate guest experiences! PC-based control for the entertainment industry

    A host of references worldwide in the areas of mobile and stationary stage and show technology, unique applications as well as the attractions industry are ample proof that PC-based control technology is ideal for implementing technically demanding stage shows and media stagings. When it comes to fast set changes, complex video projections, spectacular light shows and water features, kinetic installations, animated figures as well as interaction between the audience and media, creativity is essential on the part of the artists and designers, but also of the control technology, which quite literally brings the ideas to stage.

  • Open control technology reduces energy consumption and carbon footprint
    13.06.2025 | Application report

    Open control technology reduces energy consumption and carbon footprint
    Airwatergreen AB, Sweden

    With NEXT, the Swedish company Airwatergreen AB is breaking new ground in the dehumidification of air in industrial buildings and warehouses. The patented CVP technology reduces energy requirements and ensures an indoor climate that prevents corrosion and mold growth. PC-based control from Beckhoff regulates this innovative process and – due to its open nature – enables networking and remote maintenance of the systems, including energy tariff-optimized and thus cost-saving operation.

  • Flexible gateway due to finely scalable control technology
    13.06.2025 | Application report

    Flexible gateway due to finely scalable control technology
    Schrack Seconet, Austria

    Fire alarm systems work independently of the building automation system. Having detailed information about the state of the fire protection technology would make the work of many facility managers easier. Schrack Seconet has developed a flexible gateway using ultra-compact industrial PCs and TwinCAT from Beckhoff, which can be used to flexibly convert a customer-specific communication protocol to a wide range of transmission standards such as BACnet or OPC UA.

  • Flying into the future of building management
    02.09.2024 | Application report

    Flying into the future of building management
    ASL Group und Boolean, Belgium

    Is a fully autonomous building mere science fiction? No, it is already a reality, as the Belgian ASL Group in Liège is proving with a state-of-theart, 24/7 terminal for private flight operations. Beckhoff Solution Provider Boolean BV supported the implementation of this with end-to-end building automation.

  • Movable walls open up a dialog between high-tech and history
    16.07.2024 | Application report

    Movable walls open up a dialog between high-tech and history
    Zhejiang Dafeng Industry, China

    Zhejiang Dafeng Industry is a leading solution provider from China serving the tourism and cultural sectors. When a branch for a national pavillion in Hangzhou was built, Dafeng was contracted to develop an intelligent folding wall system. With its greenish tile surface, the installation resembles a famous landscape painting. In the synchronized movement of the 251 walls weighing several tons each, PC- and EtherCAT-based control technology from Beckhoff ensures functional safety.