A new type of modularized setup allows a more flexible installation of TwinCAT than before. Instead of the previous installation of three variants on one industrial PC, users can now select and install specific packages according to preference and update them as required. The new setup with TwinCAT Package Management enables individual and thus faster updating of individual TwinCAT components.
The setup with TwinCAT Package Management enables individual and thus faster updates of individual TwinCAT components. Customers simultaneously benefit from faster installation and shorter update times.
In this webinar, Henning Mersch from the TwinCAT Product Management division will share an overview of the novel possibilities that TwinCAT package management offers and answer any questions you may have.
An introduction to the new Build 4026 and PLC will be covered in separate webinars:
More about this video

Automaatio
TwinCAT on ainutlaatuinen automaation ohjelmistoympäristö, joka on avoin, modulaarinen ja kaikkien saatavilla. Se sisältää runsaasti toiminnallisuuksia ja laajenee jatkuvasti uusille automaation sovellusalueille.

TwinCAT
The TwinCAT software system turns almost any PC-based system into a real-time control with multiple PLC, NC, CNC and/or robotics runtime systems.

TwinCAT 3 Build 4026
More flexibility in automation development through modularity and extensions