Sídlo Česká republika
Beckhoff Automation s.r.o.

Sochorova 23
61600 Brno, Česká republika

+420 511 189 250
info.cz@beckhoff.com
www.beckhoff.com/cs-cz/

Feb 27, 2024

Standstill-free packing with XTS Track Management

XTS provides error-free production without any standstills via two valuable functions. Firstly, all products are continuously traceable in a system with an XTS. If a quality check after a process step reveals that the step has not been carried out correctly, the affected product is removed from further processing using the individually controlled movers. If, for example, a blister pack is not correctly positioned in the workpiece carrier, it passes through the sealing station without stopping and the work step is simply skipped. This saves on production resources, which has a positive impact on costs and on sustainability. XTS Track Management takes your production to the next level without downtime: defective products can be ejected using moving track sections. The software responds to the quality check error message by steering the track management section that the affected mover is on to the reject track. The reject track can be used to transport the defective product to a safe manual workstation, for example. Once it arrives, it is reworked or removed from the system, and a track management station returns the mover to the production flow. Manual intervention does not disrupt the process as it would in a conventional transport system. Track management sections can be placed at any point in the production process, and multiple sections can be attached throughout the process. The sealing machine from Koch PAC, as shown in the video, contains five track management stations.

More about this video

XTS | Linear product transport

XTS | Linear product transport

As an intelligent transport system, the eXtended Transport System enables flexible motion profiles and new types of machine concept.

Packaging machines

Packaging machines

PC-based control significantly increases the productivity and flexibility of packaging machines and lowers the consumption of resources.