Sídlo Česká republika
Beckhoff Automation s.r.o.

Sochorova 23
61600 Brno, Česká republika

+420 511 189 250
info.cz@beckhoff.com
www.beckhoff.com/cs-cz/

Jun 3, 2014

CP2xxx multi-touch built-in panel

Universal multi-touch for the complete machine. The CP2xxx panel generation from Beckhoff with industry-standard multi-touch display offers a feature-laden solution for any application.

More about this video

Průmyslové počítače (IPC)

Průmyslové počítače (IPC)

Dodáváme vhodné průmyslové počítače pro každou Vaši aplikaci – za použití nejnovějších technologií a pro jakoukoli výkonovou třídu.

Panel PCs

Panel PCs

The Beckhoff Panel PCs, in the versions as built-in devices or mounting arm devices in IP65, combine modern touch technologies with flexible computing power.

Multitouch-Panel-PCs

Multitouch-Panel-PCs

The CP2xxx and CP3xxx Panel PC series with screen sizes from 7 to 24 inches offer multi-touch technology and flexible computing power.

CP29xx, CP39xx | Multi-touch Control Panels

CP29xx, CP39xx | Multi-touch Control Panels

The Control Panel series CP29xx and CP39xx in diagonals from 7 to 24 inches offer modern multi-touch technology and flexible connection technology for distances of up to 100 meters.

Control Panels

Control Panels

As the front end of a machine, the Beckhoff Control Panels are its visual and functional business card and allow a wide range of customer-specific adaptations.

CP22xx | Multi-touch built-in Panel PC

CP22xx | Multi-touch built-in Panel PC

The CP22xx built-in Panel PC series is characterized by a modern operating concept with multi-touch display as well as an advanced, elegant device design. It is designed for installation in the front of a control cabinet. The CP22xx combine reliable Beckhoff Control Panel design with state-of-the-art Industrial PC technology. The right display size is available for every application – in landscape or portrait orientation (horizontal/vertical). With their highly integrated 3½-inch motherboards, the CP22xx built-in Industrial PCs represent a high-performance platform for machine design and plant engineering applications that can be used in conjunction with TwinCAT automation software under Windows 10 IoT Enterprise.

CP26xx | Dual-touch built-in Panel PC

CP26xx | Dual-touch built-in Panel PC

The CP26xx built-in Panel PC series is characterized by a modern operating concept with dual-touch display as well as an advanced, elegant device design. It is designed for installation in the front of a control cabinet. The CP26xx combine reliable Beckhoff Control Panel design with state-of-the-art Industrial PC technology. The right display size from 7 to 24 inches is available for every application – in landscape or portrait orientation (horizontal/vertical). With their highly integrated 3½-inch motherboards, the CP26xx built-in Industrial PCs represent a high-performance platform for machine design and plant engineering applications that can be used in conjunction with TwinCAT automation software under Windows Embedded Compact 7.

CP27xx | Fanless multi-touch built-in Panel PC

CP27xx | Fanless multi-touch built-in Panel PC

The CP27xx built-in Panel PC series is characterized by a modern operating concept with multi-touch display as well as an advanced, elegant device design. It is designed for installation in the front of a control cabinet. The CP27xx combine reliable Beckhoff Control Panel design with state-of-the-art Industrial PC technology. The right display size is available for every application. With their highly integrated 3½-inch motherboards, the CP27xx built-in Industrial PCs represent a high-performance platform for machine design and plant engineering applications that can be used, for example, in conjunction with TwinCAT automation software under Windows 10 IoT Enterprise.

CP29xx | Multi-touch built-in Control Panel

CP29xx | Multi-touch built-in Control Panel

Balance between latest PC technology and long-term availability of control components Modern Control Panel technology doesn't stop with the selection of the touch technology, which forms the basis of the operation of a machine or plant. The transmission of the image and touch signals, combined with the power supply or other digital signals, must work perfectly and continuously, both mechanically and electrically, and over long distances in the industrial environment. In order to reliably ensure this, Beckhoff installs Panel electronics that it develops and manufactures itself at the production location in Verl.

CP22xx-0020 | Multi-touch built-in Panel PC

CP22xx-0020 | Multi-touch built-in Panel PC

CP22xx-0030 | Multi-touch built-in Panel PC

CP22xx-0030 | Multi-touch built-in Panel PC

CP26xx-0000 | Panel PC with Arm® Cortex®-A8

CP26xx-0000 | Panel PC with Arm® Cortex®-A8

CP27xx-0010 | The fanless multi-touch built-in Panel PC

CP27xx-0010 | The fanless multi-touch built-in Panel PC

CP27xx-0020 | The fanless multi-touch built-in Panel PC

CP27xx-0020 | The fanless multi-touch built-in Panel PC

CP29xx-0000 | Multi-touch built-in Control Panel with DVI/USB Extended interface

CP29xx-0000 | Multi-touch built-in Control Panel with DVI/USB Extended interface

CP29xx-0010 | Multi-touch built-in Control Panel with CP-Link 4 – The One Cable Display Link

CP29xx-0010 | Multi-touch built-in Control Panel with CP-Link 4 – The One Cable Display Link