TwinCAT Chat becomes TwinCAT CoAgent! Beckhoff takes engineering to the next level with the latest innovative version of TwinCAT Chat: TwinCAT CoAgent. TwinCAT CoAgent simplifies the engineering workflow, saves time, cuts costs, and optimizes the use of resources.
More about this video

TwinCAT CoAgent
TwinCAT CoAgent offers comprehensive, intelligent support and combines state-of-the-art generative AI models with custom-developed AI agents.

TE1700 | TwinCAT 3 CoAgent
TwinCAT 3 CoAgent is the intelligent AI assistant that provides efficient support for PLC development, I/O configuration, and human-machine interface creation. Requirements can be formulated in normal language and TwinCAT CoAgent suggests suitable code and configurations, taking existing project structures into account. Flexible mode selection enables custom support based on the task at hand. In addition, TwinCAT CoAgent offers direct access to the documentation in the Beckhoff Information System and provides context-related recommendations for accelerated high-quality project implementation.

TE1000 | TwinCAT 3 Engineering
TE1000 is the TwinCAT development environment for convenient configuration of control, drive control and I/Os. In addition, the tool includes the configuration and programming of TwinSAFE, the safety solution from Beckhoff.