본사 대한민국
Beckhoff Automation Co., Ltd.

대륭테크노타운 3차 12층
가산디지털2로 115
08505 금천구, 서울특별시, 대한민국

+82 2 2107-3242
info-kr@beckhoff.com
www.beckhoff.com/ko-kr/

scheugenpflug-stage © Scheugenpflug
© Scheugenpflug

Jan 30, 2025

Automated for flexible and precise dispensing technology

PC-based control in a multifunctional cell for bonding, sealing and potting processes

The Scheugenpflug ProcessModule axis system forms the basis of Atlas Copco’s dispensing and screwing cells and a flexible integration platform for general contractors and machine builders. Precise process sequences are ensured by TwinCAT CNC and servo drive technology from Beckhoff, as exemplified by the DC803 DispensingCell.

Integrators and automation specialists require powerful dispensing solutions that can be flexibly adapted to a wide range of project requirements and integrated using the plug-and-produce solution. The Scheugenpflug ProcessModule and the DispensingCell DC803 were developed with these requirements in mind. The focus was on simple integration into a wide range of system designs and flexible data connection, a high level of dispensing quality when processing a variety of materials, short cycle times, and comprehensive process monitoring. All in all, the solutions of the Scheugenpflug product line from Atlas Copco are the result of more than 30 years of expertise in dispensing technology with advanced control technology. PC-based control from Beckhoff has been in use here since 2012. According to the Scheugenpflug experts, this PC- and EtherCAT-based control and drive technology offers an open system, fine scalability, and a broad product range which individually meets demanding customer requirements.

The Scheugenpflug multifunctional DispensingCell DC803 benefits from the flexible and open control technology from Beckhoff.
The Scheugenpflug multifunctional DispensingCell DC803 benefits from the flexible and open control technology from Beckhoff.

The central element is the axis system

The Scheugenpflug axis system is quick and easy to integrate reliably into new or existing production lines or production cells using a plug-and-produce solution. All parameters and processes relevant to bonding and potting are perfectly coordinated – independently of the rest of the machine. With its powerful axis and servo technology, the ProcessModule also offers high travel speeds and short cycle times in matrix, bead, and fill potting. Other features include high flexibility in terms of process and component parameters, the simple use of conveyor belts, and various process monitoring options. It also offers a high degree of repeatability and a precise start/stop, even for demanding applications. The inspection processes integrated into the axis system, such as scales, needle measurement and cleaning, ensure a stable process. A space-saving inspection system integrated with the dispensing head is available for real-time 360° monitoring of dispensing contours.

The ProcessModule is also used in the Scheugenpflug DispensingCell DC803 multifunctional cell. This offers the necessary flexibility to implement the increasingly demanding and individual requirements for bonding, sealing, and potting processes for medium (approx. 40,000 to 200,000) to high (approx. 200,000 to 2 million) quantities. The cell is specially designed for series production with short cycle times, particularly in the automotive, industrial electronics, and medical technology sectors. In addition to the flexible application options and the integrated additional processes, e.g., for process monitoring, it boasts a high axial load capacity and intuitive operation and programming of the dispensing processes.

Sophisticated CNC-controlled dispensing functions

The DC803 is implemented for a number of extensive automation tasks. These include open-loop and closed-loop control of the dispensing head, the high-speed gantry system with interpolated movements, product handling, and the inspection processes. The necessary computing power is provided by the ultra-compact Industrial PC C6030 which, according to the Scheugenpflug experts, was chosen primarily for its compact design as well as its high and easily scalable computing power. A CP3916 stainless steel multi-touch Control Panel connected via the CP-Link 4 one cable solution acts as the interface, providing the machine operator with a stable and robust operating concept with a long service life. For this customer-specific version, the company opted for branding with a centrally placed company logo and selected a keyboard and mouse tray for ergonomic operation. Beckhoff TwinCAT offers an open and secure architecture: Using the Automation Device Service from Beckhoff, all required data can be sent to Scheugenpflug’s own visualization system.

This example of a dispensing and potting system illustrates the complexity of the underlying process sequences.
This example of a dispensing and potting system illustrates the complexity of the underlying process sequences.

The highly precise movements that are essential for demanding dispensing applications are calculated centrally in TwinCAT CNC on the industrial PC and executed with the servo drive technology, namely for the X-, Y- and Z-axes of the ProcessModule, for the spindle axis of the dispensing head and, if required, for optional additional rotary axes. From Scheugenpflug’s point of view, the Beckhoff servo technology – which includes two AX5203 servo drives and AM8000 servomotors – offers the advantage of free and integrated configuration options using interfaces and excellent scalability with additional transformation options. In addition, it is quick, easy, and compact to install due to One Cable Technology (OCT). With its functions for safely reduced speed and a safe stop, TwinSAFE ensures safe system operation. This is implemented using the AX5805 TwinSAFE option card in the servo drive and with the EL6900 and EL1904 EtherCAT Terminals or the EP1908 EtherCAT Box as additional TwinSAFE components.

The Scheugenpflug experts agree that the company benefits from the broad Beckhoff portfolio of EtherCAT I/O components with IP20 and IP67 protection ratings. It enables flexible I/O use both in the control cabinet as well as in decentralized installation directly on the machine, with fast and space-saving wiring as a result. It also provides the necessary system openness to seamlessly integrate PROFIBUS, PROFINET, and EtherNet/IP components into the EtherCAT network with its high performance and comprehensive diagnostic options, and to flexibly integrate the multifunctional cell into larger systems.

Scheugenpflug and Atlas Copco

Scheugenpflug, the expert in automated electronic potting, has been operating under the company name Atlas Copco since the fourth quarter of 2024. It is part of the Atlas Copco Group, which brings together people, technologies, innovations, and expertise in global innovation centers. The associated Industrial Assembly Solutions (IAS) division develops technologies and solutions to optimize production processes in the electronics and automotive industries by combining automation and sustainability.